Is there a way in Niagara R2 to run a report which lists the BACnet objects’ instance numbers used in an UNC-520?

Issue

More BACnet objects are being added to a UNC-520. Is there a way in Niagara R2 to run a report that lists the BACnet objects’ instance numbers used in an UNC-520?

Product Line

TAC I/A Series

Environment

Niagara R2 all versions, UNC-520, UNC-410

Cause

NA

Resolution

Niagara does not offer a report which lists the Instance numbers already assigned in an UNC. About the only way to determine BACnet instance numbers in the UNC is to do a search of the station’s XML file using "instanceNumber" as the search criteria.