Issue
I/A Series R2 - Unable to delete users using the browser and Web User Admin screen. Users can be successfully deleted through WorkPlace Pro JDE, but not through the web browser. This occurs in R2 versions 514 and 522.
Environment
I/A Series R2, Enterprise Server
Cause
NA
Resolution
The issue is resolved in R2 versions 527 and higher. The excerpt from the R2 527/529 release notes state (Fixed - 10.1:6473 User cannot be deleted from browser when using Sun's Java Plugin). The solution is to upgrade the server to 527 or higher.