Issue
How many Echelon PCLTA & NIC709-USB's can use for one single PC
Environment
TAC Vista 5.x.x
Echelon PCLTA
NIC709-USB
Cause
Requirement to know, If we can run more than one PCLTA & NIC709-USB's on a single PC.
Resolution
There is no limitation on Echelon PCLTA & NIC709-USB's to use in single PC. As long as the PC has a slot for LTA & USB to insert then can be used.