Issue
Which signal types can be connected to a UI on a Xenta I/O Modules?
Product Line
TAC Vista
Environment
- Xenta 451A/452A, 421A/422A
Cause
UI is short for universal input, which means that these inputs are compatible with many different input types.
Resolution
Supported input signal types are:
- Thermistor: 1.8 KΩ at 25 °C or 10KΩ at 25 °C;
- Voltage: 0 to 10VDC;
- Current: 0 to 20mA;
- Digital Input.
Refer to the following link about 1.8KΩ and 10KΩ thermistor compatibility: