Replacement of Satchwell M 1201 Actuator forming part of combined Actuator / 2-port Valve Body assembly due to obsolescence.

Issue

Satchwell “M 1201” Actuator forming part of combined Actuator / 2-port Valve Body assembly requires replacement.

Product Line

Field Devices

Environment

  • Stand alone Satchwell “M 1201” Actuator forming part of combined Actuator / 2-port Valve Body assembly
  • M 1201
  • Actuator
  • 2-port
  • Valve Body

Cause

Obsolescence of Satchwell “M 1201” forming part of combined Actuator / 2-port Valve Body assembly.

Resolution

There is no direct replacement for the "M 1201" Actuator and as a result both the "M 1201" Actuator and the 2-port Valve Body to which it is connected will also require replacement. 

Replace Satchwell “M 1201” combined Actuator & 2-port Valve Body assembly with Schneider Electric MD10B-230 Actuator, LMD-MB Linkage Kit and Satchwell MB series 3-port Valve Body of appropriate size.

Details of the original Satchwell “M 1201” combined Actuator & 2-port Valve Body assembly may be viewed here.

Details of the replacement Schneider Electric MD10B-230 Actuator may be viewed here.

Details of the replacement Schneider Electric LMD-MB Linkage Kit may be viewed here.

Details of the replacement Satchwell MB 3-port Valve Body may be viewed here.

N.B.

Satchwell MB series 3-port Rotary Shoe Valve Body may be converted for use as a 2-port Zone Valve by means of the installation of a plumber’s plug in Port 3

  1. Install plumber's plug in Port 3 of MB series 3-port Rotary Shoe Valve Body.
  2. Tighten plumber's plug sufficiently to ensure PN 10 rating of Valve Body is not compromised.

It is possible that the "M 1201" Actuator may have been fitted with an Auxiliary Switch.

If so then an MD-S1 Auxiliary Switch may be fitted to the MD10B-230 Actuator if required.

Details of the MD-S1 Auxiliary Switch may be viewed here.