Issue
Several Xenta 102-AX controllers need to have the CO2 sensor shared among them in a LNS environment.
Product Line
TAC Vista
Environment
- CO2 (Carbon Dioxide)
- Xenta 102-AX
- nviCO2
- nvoCO2sensor
Cause
Properly binding a CO2 sensor output to multiple Xenta 102-AX VAVs.
Resolution
From the Xenta 102-AX VAV that is connected to the CO2 sensor, create a binding from the UnivIn3Sense function block/nvoCO2sensor, to VAV_Controller function block/nviCO2 in the receiving Xenta 102-AX VAVs.
It will also be necessary to set the send heart beats by following Values sent from a 102-AX via SNVT bindings are not making it to the receiving controller.