Replacement part for TSS100WJ and S/STAT

Issue

the STR-200 and STR-202 are the recommended replacement for TSS100WJ and S/STAT.

Product Line

TAC Vista

Environment

  • STR-200
  • STR-202
  • Xenta 102-AX
  • 7728
  • MR-VAV
  • TSS100WJ
  • S/STAT

Cause

Obsolete parts

Resolution

STR200 replaces the TTS100WJ (Temperature Sensor Only, PN)
STR202 replaces the S/STAT (Bypass button and Offset wheel)
STR200-202 can be used with the 7728, MRs, and Xenta 102-AX controllers.

STR200 . . . . . . . . . . . . . . . . . . . . . . . . 004603000
STR200-W (White) . . . . . . . . . . . . . . . . 004603010
STR202 . . . . . . . . . . . . . . . . . . . . . . . . 004603200

Full Datasheet containing additional information is located here.