Issue
Want to communicate directly to an Enterprise Server via BACnet. What need to be added / purchased for the Enterprise Server?
Product Line
TAC I/A Series
Environment
Niagara R2, (all versions), Enterprise Server
Cause
Part numbers IA-DRV-OSD and IA-BAC-500 will need to be purchased to allow direct BACnet communication to an Enterprise Server.
Part number IA-DRV-OSD provides support for 25 points each of OPC, BACnet, Modbus and SNMP. Additional point blocks of each type can be purchased to add 500 points increments. Additional BACnet points will require the purchase of the part number IA-BAC-500.
Resolution
Part numbers IA-DRV-OSD and IA-BAC-500 will need to be purchased to allow direct BACnet communication to an Enterprise Server.
Part number IA-DRV-OSD provides support for 25 points each of OPC, BACnet, Modbus and SNMP. Additional point blocks of each type can be purchased to add 500 points increments. Additional BACnet points will require the purchase of the part number IA-BAC-500