Issue
Do we need to purchase the BACnet MS/TP driver for an I/A Series G3 ENC-520?
Environment
I/A Series G3 ENC-520 / ENC-520-2-N
Cause
There is a need to integrate to BACnet MS/TP devices from an I/A Series G3 ENC-520.
Resolution
BACnet IP, BACnet Ethernet, BACnet MS/TP and LonWorks features are included as standard in the license of an I/A Series G3 ENC-520 / ENC-520-2-N. No additional purchase(s) is required for BACnet MS/TP.
There can be some confusion on this because the BACnet MS/TP driver is purchased and licensed separately for an I/A Series R2 UNC-520.