Sigma - Editing a Sigma object causes an error message. Releases before 4.05 SEB.

Issue

Editing a Sigma object causes an error message.

Product Line

Satchwell Sigma

Environment

Sigma

Object edit

4.04

4.05

Error

Cause

The network connection to a remote Sigma client fails.

Resolution

This issue is caused by a network connection failure on a remote Sigma client, and although not caused by the local client, once it has occurred, it will affect the local client as well.

The issue can be overcome by restarting the Sigma server.

To correct this issue, it is recommended that the site be upgraded to Sigma 4.05 SEB or later.

Sigma 4.05 SEB is available for download.