How to delete the photo in a personnel object without having to delete the personnel object itself.

Issue

There seems to be no way to delete the photo in a personnel object.

Product Line

Andover Continuum

Environment

CyberStation

Cause

Keep the personnel object and delete the photos in the personnel object.

Resolution

There is no way to delete the photo once it has been captured into the personnel object, a workaround is to create a blank image using an application such as Windows Paint for example and then change the personnel’s photo to the blank image.