How to determine what version of LonMaker and LNS Server on a computer.

Issue

Instructions for finding the version of LonMaker and LNS Server on a machine.

Product Line

TAC Vista, TAC I/A Series, Other

Environment

Echelon LonMaker

Cause

Knowing the version of LonMaker and LNS are necessary for many troubleshooting techniques. Support representatives may ask you to have this information available in order to assist you better.

Resolution

Please follow these steps to find the version of LonMaker and LNS server on the machine:

  1. Open LonMaker, then pick and completely open a network.
  2. Choose the LonMaker menu in the menu bar, then about LonMaker:

This is the about LonMaker window that should be shown. As you can see in this screen capture, LonMaker 3.1 is being run with the LNS server version 3.27.