Issue
When the mouse curser is hovered over bang in Continuum Explorer, the tool tip is not indicating what is wrong.
Environment
ACX57xx
Cause
Windows 7 is inhibiting tool tips on Bang indicators.
Resolution
The following registry entry is used to inhibit or expose the Tool Tips on a Mouse Over
Note: Always backup the registry before making any changes.
- HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\Advanced Data
- Type: REG_DWORD [Dword Value] // Value Name: ShowInfoTip
- Modify/Create the Value Name [ShowInfoTip] according to the Value Data listed below.
- Value Data: [0 - ShowInfoTip Disabled / 1 - ShowInfoTip Enabled]
Exit Registry and Reboot following changes to the registry.