How to determine which version of the CPU card (GCMA-112-x) of the GCM-84000 series supports the GCS bus.

Issue

How to determine which version of the CPU card (GCMA-112-x) of the GCM-84000 series supports the GCS, ASD, or other communication protocol.

Product Line

TAC I/A Series

Environment

GCMA-112-x, CPU printed circuit board for the GCM-84000 series

Cause

Cross reference purposes. 

Resolution

 

CPU Part No.

Bus Type
GCMA-112-000 GCS (standard)
GCMA-112-001 GCS (standard)
GCMA-112-002 ASD
GCMA-112-003 CCL
GCMA-112-010 GIM-21000
GCMA-112-011 GIM-MTECH

This table shows which version of the GCM CPU card supports the different firmware and bus types.