Issue
Error indicates - Invalid or inaccessible view "pxEditor:pxEditor" when attempting to view px pages through I/A Series G3 embedded Workbench via browser.
Environment
I/A Series G3 ENC
Cause
Incorrect licensing or missing pxEditor module
Resolution
-
Look in the ENC's license file under the License Manager, and look for this line:
<feature expiration="never" name="web" parts="ENC-520-WEB, ENC-WB" ui="true" ui.wb="true" ui.wb.admin="true"></feature>
If any of the "ui" fields are "false", then you need to have the ENC licensed for Embedded Workbench. Purchase part number ENC-WB. - In the Software Manager, look for a module called pxEditor. If pxEditor is not installed, install using the Commissioning Wizard.