Issue
Xenta Server Log Error contains the error line: Generic OS: Too Many Semaphores.
5326 02-Dec-2011 12:47:33 AM fatal undef httpdd 1
Generic OS: Too many semaphores. (Error#:8202)
Product Line
TAC Vista
Environment
- Xenta Server System Error Log
- Xenta 701, 711, 721, 731
Cause
An Application in Xenta 700 consumes too many internal semaphores which cause a fatal error resulting in repeated coldstarts.
Resolution
Corrected in release 5.1.0 and documented on page 6 of TPA-MALR-08-0009.00.
Upgrade to Vista version >5.1.0.