Issue
I/A Series G3 ASD driver Microzone II controller object point values indicate active override conditions when no overrides have been applied.
Environment
I/A Series G3, Microzone II, ASD, tacAsd
Cause
tacAsd driver / Microzone II firmware compatibility issue
Resolution
Due to compatibility issues, use of the tacAsd driver with Microzone II firmware below Version 2.0 will cause the associated Microzone II point values to indicate false override conditions. For proper operation, the Microzone II device firmware must be upgraded to V2.0. The V2.0 firmware kit can be ordered using part number MZ2A-119-200.