Issue
When attempting to start InVue Developer, an error message appears preventing it from proceeding:
The application cannot be edited. Process "WindowMaker" on computer "PCNAME" is editing this application.
The Invue jobsite graphics and tagname database were last modified on a different computer. Invue creates a "lock" file which prevents the application files from being changed on any other engineering computer than the original.
Environment
Wonderware for Intelligent Buildings (WIBS) or InVue version 1.1
Cause
The application (graphics generation) was done on a different computer than the current one.
Resolution
In the application directory, find and delete the appedit.lok file and re-start InVue Developer.