STR-250 functionality on Micro Regulators (MR).

Issue

Does the STR-250 work on Micro Regulators (MR)?

Product Line

TAC I/NET, TAC Vista

Environment

I/NET Seven

STR-250, I/STAT, M/STAT

I/SITE Controller and Micro Regulators (MR)

Cause

The STR-250 Wall Module is the replacement for the commonly referred to I/STAT sensor, still referenced in I/NET documentation.  The I/STAT is no longer available. 

Resolution

The STR-250 sensor is the replacement for the I/NET I/STAT, so installation and configuration for the STR-250 is as per this I/STAT. There are two documents that will provide assistance with this TCON126 and TCON299 (Chapter 21).

The STR-250 full functionality must be installed on the I/STAT port of any I/NET device and configured as detailed in the above documents. Only one I/STAT port exists per MR.

The M/STAT is still available and is used as the hardware tool for configuring the controller settings on all supported I/STAT devices, such as, all Micro Regulators (MR) variants, I/Site LAN Controller (Model 7728) and Xenta 102-AX.