How to identify the Sigma Version installed on a Computer.

Issue

Sigma software identity.

Product Line

Satchwell Sigma

Environment

Sigma
Release 1, 2, 3
Release 3.1
Release 3.3
Release 3.4
Release 3.6
Release 3.7
Release 3.7 sp2
Release 3.7 sp3
Release 3.10
Release 3.11
Release 4.00
Release 4.00 SP2
Release 4.00 SP4
Release 4.01
Release 4.01 SP1
Release 4.01 sp3
Release 4.01 sp4
Release 4.01 SP4a
Release 4.01 sp5
Release 4.02
Release 4.03
Release 4.03 sp1
Release 4.04
Release 4.04 sp1
Release 4.04 sp2
Release 4.04 sp3
Release 4.05
Release 4.05 SP1
Release 4.05 SP2
Release 4.05 SEB
Release 4.06
Release 4.07
Release 4.07 SP1
Release 4.07 SP2
Release 4.08

Build
Release
Sigma Build
Sigma release
1.52
2.13
3.12
3.12
3.17
3.3
3.31.1
3.32.10
3.33.9
3.33.11
3.33.13
3.34.11
3.34.11
3.36.11
3.36.16
3.36.20
3.37.08
3.37.09
3.37.12
3.37.13
3.37.16
3.37.18
3.39.09
3.40.06
3.40.09
3.41.14
3.41.15
3.41.16
3.41.18
3.41.19
3.42.34
3.42.43
3.42.48
3.43.18
3.44.14
3.44.16
3.44.18
3 45 48
3 45 51
3 45 58
3.46.57
3.46.62
3.46.70
3.46.72
3.46.73
3.46.79
3.46.80
3.46.81
3.46.85
3.46.86
3.46.89
3.46.98
3.46.104
3.46.105
3.46.107

Cause

Software installs with a build number and not a release number.

Resolution

To view the Sigma build number select About System Manager from the Help menu

 

The displayed window shows the Sigma build number

Refer to the table below to find the Release No.

   LL Article 6748   Last Updated: 2017-08-11 Logo_SE_Green.jpg
 
   Sigma Release No. Build No. Software/Firmware File Date SigmaX
         
Release 1 1.52 Software/Firmware 22.06.2001 SigmaX 4.5
Release 2 2.13 Software/Firmware 14.02.2002 SigmaX 5.2
Release 2 3.12 Supplement 14.02.2002 SigmaX 5.2
Release 3 3.12 Software 31.07.2002 SigmaX 5.2
Release 3.1 3.17 Software 17.09.2002 SigmaX 5.2
Release 3.3 3.3 Software 30.07.2003 SigmaX 5.2
Release 3.4 3.31.1 Software 03.10.2003 SigmaX 5.2
Release 3.6 3.32.10 Software 19.11.2003 SigmaX 5.2
Release 3.7 3.33.9 Software 22.12.2003 SigmaX 5.2
Release 3.7 SP2 3.33.11 Software 27.01.2004 SigmaX 5.2
Release 3.7 SP3 3.33.13 Software 19.02.2004 SigmaX 5.2
Release 3.10 3.34.11 Software 21.04.2004 SigmaX 5.2
Release 3.11 3.34.11 Supplement 31.08.2004 SigmaX 5.2
Release 4.00 3.36.11 Software 16.12.2005 SigmaX 6.0.1
Release 4.00 SP2 3.36.16 Software 02 03 2006 SigmaX 6.0.1
Release 4.00 SP4 3.36.20 Software 23.05.2006 SigmaX 6.0.1
Release 4.01 3.37.08 Software 07.09.2006 SigmaX 6.0.1
Release 4.01 SP1 3.37.09 Software 26 09 2006 SigmaX 6.0.1
Release 4.01 SP3 3.37.12 Software 20 10 2006 SigmaX 6.0.1
Release 4.01 SP4 3.37.13 Software 13 08 2006 SigmaX 6.0.1
Release 4.01 SP4a 3.37.16 Software 17 11 2006 SigmaX 6.0.1
Release 4.01 SP5 3.37.18 Software 05 01 2007 SigmaX 6.0.1
Release 4.02 3.39.09 Software 26 01 2007 SigmaX 6.0.1
Release 4.03 3.40.06 Software 06 06 2007 SigmaX 6.0.1
Release 4.03 Sp1 3.40.09 Software 09 08 2007 SigmaX 6.0.1
Release 4.04 3.41.14 Software 27.02.2008 SigmaX 6.0.1
Release 4.04 SP1 3.41.15 Software 09.05.2008 SigmaX 6.0.1
Release 4.04 SP2 3.41.16 Software 15 09 2008 SigmaX 6.0.1
Release 4.04 SP3 3.41.18 Software 08 01 2009 SigmaX 6.0.1
Release 4.04 SP4 3.41.19 Software 08 01 2009 SigmaX 6.0.1
Release 4.05 3.42.34 Software 06 11 2009 SigmaX 6.0.1
Release 4.05 SP1 3.42.43 Software 22 03 2010 SigmaX 6.0.2
Release 4.05 SP2 3.42.48 Software 26.08.2010 SigmaX 6.0.2
Release 4.05 SEB 3.43.18 Software 08 12 2010 SigmaX 6.0.2
Release 4.06 3.44.14 Software 01 12 2011 SigmaX 6.0.2
Release 4.06 SP1 3.44.16 Software 01 12 2011 SigmaX 6.0.2
Release 4.06 SP1 3.44.18 Hotfix 01 02 2012 SigmaX 6.0.2
Release 4.07 3 45 48 Software 20 08 2012 SigmaX 7.0.6
Release 4.07 SP1 3 45 51 Service Pack 09 12 2012 SigmaX 7.0.6
Release 4.07 SP2 3 45 58 Service Pack 20 12 2013 SigmaX 7.0.6
Release 4.08 3.46.57 Software 10 04 2014 SigmaX 7.0.7
Release 4.08 3.46.62 Hotfix 21.05.2014 SigmaX 7.0.7
Release 4.08 3.46.70 Hotfix 23 07 2014 SigmaX 7.0.7
Release 4.08 3.46.72 Hotfix 04 08 2014 SigmaX 7.0.7
Release 4.08 3.46.73 Hotfix 12 08 2014 SigmaX 7.0.7
Release 4.08 3.46.79 Hotfix 08 10 2014 SigmaX 7.0.7
Release 4.08 (**1) 3.46.80 Software 10 04 2014 SigmaX 7.0.7
Release 4.08 3.46.81 Hotfix 17 02 2015 SigmaX 7.0.7
Release 4.08 3.46.85 Hotfix 19 03 2015 SigmaX 7.0.7
Release 4.08 3.46.86 Hotfix 19 03 2015 SigmaX 7.0.7
Release 4.08 (**2) 3.46.89 Software 10 04 2014 SigmaX 7.0.7
Release 4.08 3.46.98 Hotfix 14 12 2016 SigmaX 7.0.7
Release 4.08 (**3) 3.46.104 Software 28 02 2017 SigmaX 7.0.9
Release 4.08 (**4) 3.46.105 Hotfix 28 03 2017 SigmaX 7.0.9
Release 4.08 3.46.107 Hotfix 08 08 2017 SigmaX 7.0.9
Notes:        
**1 Sigma 4.46.57 with StruxureWare Building Operation v1.5 or 1.6 Support Programme installed.
**2 Sigma 4.46.57 with StruxureWare Building Operation v1.8 Support Programme installed.
**3 Sigma 4.46.57 with StruxureWare Building Operation v1.9 Support Programme installed.
**4 Sigma 4.46.57 with StruxureWare Building Operation v1.9 Hotfix to Support Programme installed.

 

2015-01-21 Note:
Sigma X version 7.0.9 is now available and can be used on any Sigma version that supported Sigma X verison 7.0.6.

If you would like to view this information Click Here (Opens in new tab/window)

If you would like to download this information as a PDF file Click Here

Note: -
When SigmaX 6.0.2 is installed, the build information provided by Sigma (Help > About) can be wrong (later than the actual version).This arises because SigmaX installs a file with Build 3.42.47 in the c:\Sigma\bin folder. This is only a problem prior to Sigma Release 4.05 SEB.