What 10K Thermistor sensors are compatible with the I/A Series R2 UNC-410 and G3 ENC-410?

Issue

What 10K Thermistor sensors are compatible with the I/A Series R2 UNC-410 and G3 ENC-410?

Product Line

TAC I/A Series

Environment

I/A Series R2, UNC-410, I/A Series G3, ENC-410

Cause

Specification information

Resolution

Compatible sensors include the TS-5700, TS-5711, TS-57011, TS-57031, TS-6700, TSMN-90110 Series, or any sensor that matches the resistance to temperature curve for a 10K Thermistor Type G.  The input has a range of -10 to 135 °F (-23.3 to 57.2 °C) with an accuracy of ±1% of span.

Note: Network 8000 sensors (10K with the 11K shunt) are not compatible.

US Sensor 10K Thermistor R-T Curve Type G