Is there an Xdriver Error Log?

Issue

I can see the XdriverError count but where is the corresponding log?

Product Line

Andover Continuum

Environment

XDriver

Cause

The xDriver tab indicates the count or errors and the last error but where is the error log?

Resolution

For 1st generation controllers the last error should be shown in the comm port status. There is no error log. A PE program can be written to map this attribute to an InfinityString to create a log.

For 2nd generation controllers (like the NCII) the errorlog function does not work correctly.  The ErrorLogTool.exe must be used to extract this information.