Issue
When converting controller type in Continuum such as making a CX9900 (NC1) into a CX9680 (NC2) if the System Variable objects contain links such as triggers or alarms and/or configuration edits such as logs etc those links and configuration edits will be lost during the conversion.
Environment
CyberStation
Cause
Implementation
Resolution
Before converting the controller, in the Continuum Explorer click on the System Variables folder and then select ALL the system variable objects on the right pane and export them to a text file.
After the conversion is done, import the system variables to restore all triggers/links etc.