Issue
There is a 24 character limit for an expression when entered through Epibuilder>layout properties>Encoding> Field Expression
Environment
- Cyberstation
- webClient
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
ImageWare EpiBuilder has limited this way of entering in the expression, but offers another method for a work around.
Resolution
To work around this limitation issue.
-
Define the expression first in the following place Edit> Define Expression
Ex. [Info1]+[Info2]+[Info3]+[Info4] - Click OK
- Layout Properties> Encoding> Field Expression
- The drop down now contains [Info1]+[Info2]+[Info3]+[Info4] which could not be entered directly.