I/A Series (Niagara) AX/G3/N4 Windows Compatibility Matrix

Issue

Is the I/A Series AX/G3/N4 software compatible with a specific version of Windows?

Product Line

TAC I/A Series

Environment

 I/A Series (Niagara) AX/G3/N4 software

Windows 32-bit and 64-bit operating systems

Cause

 Only specific releases of the I/A Series AX/G3/N4 software have been certified compliant with specific versions of the Microsoft Windows software. 

Resolution

The following chart details the version compatibility between the releases of the I/A Series G3 software and various versions of the Microsoft Windows Operating System software.

UPDATE:  CLICK HERE TO VIEW LATEST RELEASE COMPATIBILITY MATRIX AS OF March 2018

UPDATE:  CLICK HERE TO VIEW EARLIER RELEASE COMPATIBILITY MATRIX

^ 64-bit LON client not available; 64-bit serial client available in 3.6.47, 3.7, and 3.8

* Refer to PA-00163 for Windows 7 Support Info
 

For the larger Schneider Electric BMS offering please refer to Lessons Learned Article 4240