Issue
When trying to backup an I/A Series R2 UNC (Niagara) station, receive an error,
"*** BACKING UP: Station Name [192.168.7.242]
*** FAILED: Station Name [192.168.7.242]: java.lang.NullPointerException"
Environment
I/A Series R2 UNC (Niagara) station
Cause
One cause of this error is that all of the Threads are being used.
Resolution
1. Increase Thread Count from 15 to 30 (Admin Tool - Host - Edit File - System Properties)
2. Reboot the UNC