24 hour Vista log does not collect information.

Issue

When a log is defined in Vista for a 24 hour log period no values are logged.

Product Line

TAC Vista

Environment

Vista 5.1.6.

Windows 7 32 bit

Cause

There is a known issue with Vista 5.1.6 and time zones of the Vista server PC.

24 Hour logs do not start to collect information if the time zone is set to GMT +2 or greater.

Resolution

The only resolution currently is to change the log to 12 hourly.

Then use Excel to add these together if this value is used in a Report.

This problem has been fixed in the release of Vista 5.1.6. Upgrading to this version will fix the problem.