What is the accuracy of the MN-S wall sensor for Micronet 2000?

Issue

What is the accuracy of the wall sensors used with the Micronet 2000 controllers?  The sensor model numbers are:  MN-S and MN-SDK.

Product Line

TAC I/A Series

Environment

Micronet 2000

Cause

Required for a job submittal

Resolution

Click here to view Technical Bulletin 97_35 which provides sensor accuracy details.