Is there a field upgrade kit to add the UPS option to the Continuum power supply?

Issue

Can the UPS option be added to an existing Continuum power supply?

Product Line

Andover Continuum

Environment

Continuum Power Supply

PS120/240-AC85

Cause

Can the UPS option be added in the field to a Continuum PS120/240-AC85?

Resolution

No. There is no field upgrade kit to add the UPS option to a Continuum power supply.