Issue
I/A Series R2 UNC-600 and UNC-610 BIOS Settings and CMOS Battery Replacement
Environment
I/A Series R2 UNC-600 and UNC-610
Cause
NA
Resolution
The following publication describes the BIOS settings required when replacing the CMOS battery in the UNC-600 or UNC-610. Be extremely cautious when replacing the battery as the battery holder can become very brittle with age.
TB06-05_UNC6x0_Bios_settings_and_CMOS_Battery_Replacement.pdf