How to clear the controller flash backup from the hardware using the reset IP switch.

Issue

How to clear the controller flash backup from the hardware using the reset IP switch.

Product Line

Andover Continuum

Environment

CX9640

CX9680

CX5720/40

Cause

Need to remove any backup in flash but has no access to the controller's web page configuration.

Resolution

Pushing and holding down the controller's reset IP switch for 30 seconds clears any backup of the database in flash in addition to resetting the IP address and ACC node id.