Issue
The option to add or decrease the number of remote I/O modules using the Remote IO Wizard is shown, but what is the process to eliminate all modules?
Environment
I/A Series WorkPlace Tech
Cause
Eliminate all I/O modules using the Remote IO Wizard
Resolution
- Open the ADI/Remote IO Wizard from the Applications menu.
- With the Remote IO Wizard window displayed hit the Back button and select "none" and click Next.
-
When prompted with "Do you wish to continue?" select yes and all the RIO Input and output tags will be removed from the drawing.
Note: objects that were linked to these tags that are no longer being used must be "cut" from the drawing manually.