Issue
The Link tab in Schedule Object shows " Prism Error "
Environment
R2 Niagara
Cause
Directly linking the schedule or calendar status output via external link to another station may cause the receiving station's object to not follow the associated calendar or schedule event. The link tab will show "Prism Error"
Resolution
The schedule object output should only be linked to objects within the station and not between stations. Schedule and calendar objects between stations should only be linked via the master/slave links.