Issue
video layout stub error exception pops up when a video layout is triggered to pop up on alarm
Exception error: object reference not set to an instance of and object
Environment
- Continuum
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
- In some cases having a layout populated with 6 or more cameras may show the error.
- A remote connection opening a video layout at a quick pace can cause this.
Resolution
- If you are using 1.92 upgrade to 1.93
- If you are using a remote connection, the same error will not pop up from the local PC.