Issue
Get "Value does not fall within expected range" error message when trying to view values from a Vista node in webstation.
Environment
- Vista 5.1.X
- Webstation 5.1.X
- Vista in network (master with at least 1 slave)
Cause
This is a COM error caused by a difference in regional settings on the Vista servers. E.g. 100 000.00 may be retrieved as 100,000.00 if other settings are used on another server. This will cause a mismatch.
Resolution
Ensure that the settings for digit grouping and decimal symbol are the same on all Vista servers.
- Click on Start\Control Panel\Regional and language options.
-
Select Customize and check the settings on the Numbers tab.
- Compare these settings with the other Vista servers.