Issue
Will NC2/ACX2 controller warm or cool start after its IP address is changed from the configuration web page?
or is it the case that the controller must be reloaded?
Environment
CX9640
CX9680
ACX5720
ACX5740
Cause
Function as designed
Resolution
Changing the IP address or ACCNetId of a 9640/9680 or ACX5720/40 invalidates the backup in the controller's flash memory.
Controller will have to be reloaded from CyberStation after it re-starts.