Issue
How to re-create the default objects such as default list views and alarm enrollments.
Environment
CyberStation
Cause
Not known cause
Resolution
Run the Continuum database initialization utility then go to the server or stand alone tab (depending on your configuration).
Tick the Create Default List Views check box and/or any of the other check boxes that create default objects.
Make sure the Update Existing Database is selected in the create or update group.
Click Continue to update the database and create the default objects.