Is there a way to determine who is actively logged into CyberStation and onto which workstation?

Issue

How to determine who is logged into the Continuum system and onto which workstation?

Product Line

Andover Continuum

Environment

CyberStation

Cause

Is it possible to see via a Listview or Pinpoint who is logged into Continuum and onto which workstation?  

Resolution

There is no "live" means to see who is logged into what workstation. However, a listview of ActivityEvent filtered by today and action code 15 and 16 and auto-refreshing every 30 seconds is pretty close. This listview will show what user logged in and when to which workstation. It will show the same information for users logging off. So one can deduce who is currently on which workstation.

Simply download and unzip this dump file and import it into the root of Continuum Explorer and run it.