Issue
- What is Xenta 28x, 30x, 401 web and Xenta 28x, 30x, 401 TCP/IP
- Is there any documentation for 28x, 30x, 401 web and Xenta 28x,30x, 401 TCP/IP
Environment
Xenta 281 Web
Xenta 282 Web
Xenta 301 Web
Xenta 302 Web
Xenta 401 Web
Xenta 281 TCP/IP
Xenta 282 TCP/IP
Xenta 301 TCP/IP
Xenta 302 TCP/IP
Xenta 401 TCP/IP
Cause
These are not products they are packages.
Resolution
The Xenta 280, 30x, 401 web and TCP/IP are not a controller type. It is just a packaging.
The 280, 30x, 401 TCP/IP is sold with a Xenta 911 and the Xenta 280,30x, 401 Web are sold with a Xenta 511.
So the documentation for "normal" Xenta 280 and Xenta 911/511 is used. This can be found on the Exchange Extranet.