Issue
An issue has been identified where the holiday schedule dates do not fit in the display windows when using Windows 7. This was reported on Sigma Build 3.42.43. The latest release has been tested and the same issue is present.
Environment
Sigma
Cause
Windows 7 Screen setting
Resolution
This will be reported as a minor fault. There is a workaround for this. The screen needs to be set to windows classic which replicates the Windows XP display windows.
To do this:
- Right-click on the desktop
- Select "Personalize"
- Scroll to the bottom windows and select "Windows Classic".
- This will then change the display and the holiday schedule will display correctly