Is there a recommended repeater for BACnet MSTP networks?

Issue

Is there a recommended  repeater for BACnet MSTP networks?

Product Line

TAC I/A Series

Environment

I/A Series R2 G3 (Niagara) MNB-1000

Cause

MSTP repeaters may be required to extend trunk length or provide isolation as in the smoke purge application.

Resolution

Consider the B-LINK-AC-S (AC powered) or B-LINK-DC-S (DC powered) that was used on the MSTP trunk during UL 864 testing. 

There is also a fiber repeater available:  B-LINK-F-DC-S