Issue
Cannot open a Niagara G3 station with via a web browser
Environment
Niagara G3 all versions, ENC-520, ENC-410, ENS
Cause
The station’s HTTP port number was changed from it default port number of 80.
Resolution
If the station’s HTTP port number was changed to something other than the default port number 80, then the HTTP port number must be included with the station IP address in the web browser URL
Example:
A station’s HTTP port was changed from its default 80 to 8080.
The following will need to be entered into the web browser’s URL in order to gain access to the station:
http://<station IP address>:8080