Where do I obtain the documentation for the I/A Series G3 Schneider Electric proprietary drivers?

Issue

The documentation for the I/A Series G3 Schneider Electric (TAC) proprietary drivers are not included with the I/A Series G3 software documentation.  Where can those documents be obtained?

Product Line

TAC I/A Series

Environment

I/A Series G3 ASD Driver

I/A Series G3 GCM Driver

I/A Series G3 MicroSmart Driver

I/A Series G3 DMS Driver

Cause

Documentation for these drivers is not included with the I/A Series G3 software release

Resolution

The documentation for the I/A Series G3 Schneider Electric (TAC) proprietary drivers can be downloaded from the Publication Zone (under Links) on iPortal (http://usiportal.tac.com).  The following documents are available:

F-27522 -- I/A Series G3 ASD Driver

F-27527 -- I/A Series G3 GCM Driver

F-27523 -- I/A Series G3 MicroSmart Driver

F-27541 -- I/A Series G3 DMS Driver