Issue
Reloading a BCX4040 causes it to appear offline.
Environment
bCX4040
Cause
After a reload, a bCX is offline.
Resolution
- Dump bCX to text file.
- Delete bCX from CyberStation.
- Clear database backup via controller webpage.
- Add back the bCX in CyberStation and performed a Teach.
- In global BACnet Preferences (Cyber icon in Windows tray), add BBMD information and run Teach in the BBMD Registration editor.
- Import the dump file from Step 1.
- Perform a successful reload.