Are there I/A Series R2 and G3 objects for interface with the SE7000 Series Room Controllers?

Issue


Are there I/A Series R2 and G3 objects for interface with the SE7000 Series Room Controllers?

Product Line

TAC I/A Series, Field Devices, SmartStruxure Lite

Environment

I/A Series R2 and G3, SE7000 Series Room Controller

Cause

Not able to locate shadow objects with matching LonWorks program IDs within the existing I/A Series R2 and G3 modules.

Resolution

A set of new modules have been generated for use with the new SE7000 Series Room Controllers.  The new objects interface with the following program IDs.

R2 objects:

Se7273         (80:00:10:55:00:04:04:20)
Se76Pir         (80:00:10:55:00:04:04:21)
Se76RhPir    (80:00:10:55:00:04:04:22)

Click to download ... lonSchneider-2.301.330.zip
Click to download ... lonSchneider-2.301.431.zip
Click to download ... lonSchneider-2.301.534.zip

G3 objects:

Se72_73.lnml (80:00:10:55:00:04:04:20)
Se76Pir.lnml (80:00:10:55:00:04:04:21)
Se76RhPir.lnml (80:00:10:55:00:04:04:22)

Click to download ... lonSchneider-3.5.39.1.zip
Click to download ... lonSchneider-3.7.17.zip

The 3.5.39.1 module should be used with G3 versions 3.5 and lower.
The 3.7.17 module should be used with G3 versions 3.6 and higher.