Replacement of VTRA Valve Body by VTRE or MB/MBF Valve Body due to obsolescence.

Issue

VTRA Valve Body requires replacement due to obsolescence.

Product Line

Field Devices

Environment

  • VTRA
  • 3-port Mixing Valve Body

Cause

Obsolescence of VTRA Valve Body

Resolution

VTRA Valve Bodies are obsolete and have been for many years.

VTRA Valve Bodies were available with either Flanged or Screwed connections.  Details of the various size / connection combinations available appear here.

REPLACEMENT OF VTRA FLANGED CONNECTION VALVE BODY

A replacement for the VTRA Flanged Valve Body (32-80mm) may be selected from the VTRE range of Flanged Valve Bodies, details of which appear here.

N.B.

It should be noted that the VTRE Valve Body is rated PN6 whereas the VTRA was rated PN10.

The VTRE Flanged Valve Body may be operated by the EM9 Actuator, details of which appear here.

Alternatively the VTRE Flanged Valve Body may be operated by the M9B Actuator, details of which appear here.

No Linkage Kit is required to mount the EM9 or M9B Actuator on the VTRE Valve Body.

Alternatively a replacement for the VTRA Flanged Valve Body (65-80mm only) may be selected from the MBF range of Flanged Valve Bodies, details of which appear here.

N.B.

It should be noted that the MBF Valve Body is rated PN6 whereas the VTRA was rated PN10.

The MBF Flanged Valve Body may be operated by the MD20B series Actuator, details of which appear here.

Alternatively the MBF Flanged Valve Body may be operated by the MD20A Actuator, details of which appear here.

A Linkage Kit (914-1070-000) will also be required, details of which appear here.

 

REPLACEMENT OF VTRA SCREWED CONNECTION VALVE BODY

A replacement for the VTRA Screwed Valve Body (15-50mm) may be selected from the MB range of Screwed Valve Bodies, details of which appear here.

The MB Screwed Valve Body may be operated by the MD10B series Actuator, details of which appear here.

Alternatively the MB Screwed Valve Body may be operated by the MD10A Actuator, details of which appear here.

A Linkage Kit (914-1071-000) will also be required, details of which appear here.