Issue
Graphics not functioning after moving I/NET to a new machine that uses direct serial connection
Points are not displaying data but links between pages still work.
Environment
I/NET Seven
Direct Connect
Cause
I/NET link and station numbers must be correct for I/NET graphics to work
Resolution
You can verify that this is the issue by editing a graphic and determine the link address of a displayed point. If this link is not available when you try to connect to the controller then you will need to change your I/NET configuration.
- Open I/NET Configuration
- Modify the Active Profile
- Ensure that the System and Hardware Addresses configured match the configuration of the original computer