Issue
In Vista 4.5 it is not possible to acknowledge a alarm logged in as a Field user from Webstation, is this possible in Vista 5.1.6?
Environment
Vista and Webstation 5.1.6
Cause
In Vista 5.1.6 it is possible to acknowledge alarms even with a Field user.
Resolution
Upgrade from Vista 4.5 to Vista 5.1.6