Different Forta versions.

Issue

There are different versions of TAC Forta actuators available on the global market.

Product Line

Field Devices

Environment

Forta actuators on the global market.

M400

M400A

M800

M800A

M1500

M1500A

Cause

There are different types of Fortas available.

Resolution

The "A" version of the Forta actuators are designed to be used on the US market. There are several differences between the "A" series and the regular type, but the key ones are:

-UL approval

-Electrical connections designed to conform to US standards

-The VB version is equipped with a short yoke to fit directly on the VB series of valves used on the US market.