Issue
Customize the default graphic that opens after login.
Environment
- Vista Workstation
- Vista Webstation
Cause
Vista defaults to a generic view which can be customized.
Resolution
The Home Graphic can be changed in any user profile, including the default Vista $UserProfile. A user profile can be used by several users.
To create a User Profile
- In the folders pane, right-click the root object.
- Point to New, point to Object, and then click User Profile.
- Type the name of the object.
Browse the Home Graphic in the new User Profile and update each User properties to use the correct User Profile.